UserDefined Enumeration¶
-
class
NXOpen.Routing.
UserDefined
¶ Bases:
object
Option to indicate if an existing
NXOpen.Routing.LineSegment
,NXOpen.Routing.ArcSegment
orNXOpen.Routing.SplineSegment
is user defined. Enum MembersEnum Member Enum Member Description NotUserDefined System generated segment. System manages simplification and some update behavior. UserDefined User defined generated segment. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-