Terminal Enumeration¶
-
class
NXOpen.Routing.
Terminal
¶ Bases:
object
Option to query if an existing
NXOpen.Routing.ISegment
is a terminal segment. Enum MembersEnum Member Enum Member Description NotTerminalSeg Is not a terminal segment TerminalSeg Is a terminal segment -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-