StockStyleBuilderStockStyle Enumeration

NXOpen.Routing.StockStyleBuilder.StockStyle is an alias for NXOpen.Routing.StockStyleBuilderStockStyle

class NXOpen.Routing.StockStyleBuilderStockStyle

Bases: object

Enum to define the stock style

Enum Members

Enum Member Enum Member Description
Centerline
SimpleSolid
DetailedSolid
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.