StockDataRefreshBuilderRefreshStatus Enumeration¶
NXOpen.Routing.StockDataRefreshBuilder.RefreshStatus is an alias for NXOpen.Routing.StockDataRefreshBuilderRefreshStatus
-
class
NXOpen.Routing.
StockDataRefreshBuilderRefreshStatus
¶ Bases:
object
The stock data refresh status
New in version NX12.0.0.
Enum Members
Enum Member Enum Member Description Ok Refresh successful StockDataTagInvalid NULL stock definition encountered StockDataMissingSearchAttributes No attributes used for searching library found StockPartNotFoundInReuseLibrary Cannot find stock under the stock or overstock root nodes in the Reuse Library MultipleStocksFoundInReuseLibrary More than one stock found - cannot resolve ambiguity StockPartNotRequired Stock part name not found indicating there is no stock part StockPartNotFoundForLoading Problem loading the stock part CannotFullyLoadStockPart Unable to fully load the stock part StockDataNotFoundInLoadedPart Unable to find a stock definition in the loaded stock part StockConversionError Error converting units of loaded stock part to that of stock definition being refreshed ErrorRefreshUndone Error encountered after partial update of stock definition; UNDO was performed to return to original state -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-