SplitDuctBuilderFlowTypes Enumeration¶
NXOpen.Routing.SplitDuctBuilder.FlowTypes is an alias for NXOpen.Routing.SplitDuctBuilderFlowTypes
-
class
NXOpen.Routing.
SplitDuctBuilderFlowTypes
¶ Bases:
object
The type of flow, whether Absolute or Relative, to be displayed in the %Flow column in the list. This also controls the type of flow based on which divisions can be created or edited
Enum Members
Enum Member Enum Member Description AbsoluteFlow Absolute flow RelativeFlow Relative flow -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-