SplinePathBuilderSplinePathSlackType Enumeration¶
NXOpen.Routing.SplinePathBuilder.SplinePathSlackType is an alias for NXOpen.Routing.SplinePathBuilderSplinePathSlackType
-
class
NXOpen.Routing.
SplinePathBuilderSplinePathSlackType
¶ Bases:
object
Describes the type of slack to be applied to the spline.
Enum Members
Enum Member Enum Member Description PercentLength The length of the spline is increased by a percentage of the spline length. AdditionalLength The length of the spline is increased by an additional length. LockLength The length of the spline is slacking to a specified and locked length. Undefined Slack length is undefined. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-