SplinePathBuilderSplinePathRadiusSource Enumeration¶
NXOpen.Routing.SplinePathBuilder.SplinePathRadiusSource is an alias for NXOpen.Routing.SplinePathBuilderSplinePathRadiusSource
-
class
NXOpen.Routing.
SplinePathBuilderSplinePathRadiusSource
¶ Bases:
object
Describes the method for the constrained curvature spline to be defined as.
Enum Members
Enum Member Enum Member Description Expression Specify radius by value. RatioToDiameter Specify radius by ratio to stock. Attribute Specify radius by attribute. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-