SplinePathBuilderSplinePathAttributeOptions Enumeration¶
NXOpen.Routing.SplinePathBuilder.SplinePathAttributeOptions is an alias for NXOpen.Routing.SplinePathBuilderSplinePathAttributeOptions
-
class
NXOpen.Routing.
SplinePathBuilderSplinePathAttributeOptions
¶ Bases:
object
Describes user attribute methods options. These value are used to set minimum checking method. If checking method is ratio to diameter than allowable radius will be computed by ratioToDiameter x Stock Diameter.
Enum Members
Enum Member Enum Member Description Radius A radius method option for spline user attribute RatioToDiameter A ratio to diameter method option for spline user attribute. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-