SplinePathBuilderDragMode Enumeration¶
NXOpen.Routing.SplinePathBuilder.DragMode is an alias for NXOpen.Routing.SplinePathBuilderDragMode
-
class
NXOpen.Routing.
SplinePathBuilderDragMode
¶ Bases:
object
Specifies if drag network is active when updating the position of a defining point.
Enum Members
Enum Member Enum Member Description Active The drag network is active Inactive The drag network is inactive -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-