SplinePathBuilderDefiningTypes Enumeration¶
NXOpen.Routing.SplinePathBuilder.DefiningTypes is an alias for NXOpen.Routing.SplinePathBuilderDefiningTypes
-
class
NXOpen.Routing.
SplinePathBuilderDefiningTypes
¶ Bases:
object
Specifies how the spline points define the shape of the spline.
Enum Members
Enum Member Enum Member Description Unsupported The defining type is unsupported. Interpolation The defining type represents a C1-continuous, interpolation spline. Parametric The defining type represents a G1-continuous, parametric curve. Bezier The defining type represents a G1-continuous, piecewise cubic Bezier. BezierSlack The defining type represents a G1-continuous, piecewise cubic Bezier with pseudo gravity slack. BezierMaxCurvature The defining type represents a G1-continuous, piecewise cubic Bezier with bounded maximum curvature. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-