SegmentManagerSubdivideSpacing Enumeration¶
NXOpen.Routing.SegmentManager.SubdivideSpacing is an alias for NXOpen.Routing.SegmentManagerSubdivideSpacing
-
class
NXOpen.Routing.
SegmentManagerSubdivideSpacing
¶ Bases:
object
Specifies spacing option for subdivide segment.
Enum Members
Enum Member Enum Member Description ScreenPoint Screen Point EqualArcLength Equal Arc Length EqualParameter Equal Parameter IncrementalArcLength Incremental Arc Length GeometricRatio Geometric Progression Ratio ChordalTolerance Chordal Tolerance NumberOfOptions Number of Options -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-