RoutingBulkReplacementBuilderRetainReasonType Enumeration¶
-
class
NXOpen.Routing.
RoutingBulkReplacementBuilderRetainReasonType
¶ Bases:
object
Defines the reason why the object has been retained. Unspecified, explicit, block unify, non-classification, and equipment Enum Members
Enum Member Enum Member Description Unspecified Retain reason is not specified Explicit Retain reason is the user explicitly marked it retain BlockUnify Retain reason is because of the presence of the NX_BLOCK_UNIFY attribute NonClassification Retain reason is the object did not originate from classification and is not supported Equipment Retain reason is the object is equipment and is not supported -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-