RoutingBulkReplacementBuilderReplacementMethodType Enumeration¶
-
class
NXOpen.Routing.
RoutingBulkReplacementBuilderReplacementMethodType
¶ Bases:
object
Defines the replacement method type. Attribute values, library select, and retain Enum Members
Enum Member Enum Member Description AttributeValues Search for a replacement object using attribute values LibrarySelect Select a replacement object from the part library Retain Keep the original object, no replacement is performed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-