RoutePartDescriptorSourceType Enumeration

NXOpen.Routing.RoutePartDescriptor.SourceType is an alias for NXOpen.Routing.RoutePartDescriptorSourceType

class NXOpen.Routing.RoutePartDescriptorSourceType

Bases: object

Descriptor Type for a NXOpen.Routing.RoutePartDescriptor.

Enum Members

Enum Member Enum Member Description
Null
PartAttribute
Expression
DumbCopy
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.