RouteManagerPartType Enumeration

NXOpen.Routing.RouteManager.PartType is an alias for NXOpen.Routing.RouteManagerPartType

class NXOpen.Routing.RouteManagerPartType

Bases: object

Collector types for Routing information

Enum Members

Enum Member Enum Member Description
Part
Stock
Fabrication
StockComponent
WireComponent
Overstock
Logical
TemplateAssy
Connector
Splice
Device
Filler
Unknown
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.