RouteManagerFindObjectType Enumeration¶
NXOpen.Routing.RouteManager.FindObjectType is an alias for NXOpen.Routing.RouteManagerFindObjectType
-
class
NXOpen.Routing.
RouteManagerFindObjectType
¶ Bases:
object
The types of objects for which FindRoutingObject will search.
Enum Members
Enum Member Enum Member Description Harness Cable Shield Connector Device Connection Wire Unknown -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-