RouteManagerBomLevel Enumeration

NXOpen.Routing.RouteManager.BomLevel is an alias for NXOpen.Routing.RouteManagerBomLevel

class NXOpen.Routing.RouteManagerBomLevel

Bases: object

Describes how fabrications are reported on the Bill of Material (BOM).

Enum Members

Enum Member Enum Member Description
Summery
Itemized
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.