RouteManagerBomFabrication Enumeration

NXOpen.Routing.RouteManager.BomFabrication is an alias for NXOpen.Routing.RouteManagerBomFabrication

class NXOpen.Routing.RouteManagerBomFabrication

Bases: object

Is the fabrication numbering option on or off?

Enum Members

Enum Member Enum Member Description
Off
On
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.