ReuseLibraryReportInBom Enumeration¶
NXOpen.Routing.ReuseLibrary.ReportInBom is an alias for NXOpen.Routing.ReuseLibraryReportInBom
-
class
NXOpen.Routing.
ReuseLibraryReportInBom
¶ Bases:
object
Represents the report in BOM logical type.
Enum Members
Enum Member Enum Member Description DoNotReport Do not report in the Bill of Materials Report Report in the Bill of Materials -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-