ReuseLibraryPartType Enumeration¶
NXOpen.Routing.ReuseLibrary.PartType is an alias for NXOpen.Routing.ReuseLibraryPartType
-
class
NXOpen.Routing.
ReuseLibraryPartType
¶ Bases:
object
Represents the part type.
Enum Members
Enum Member Enum Member Description Gasket Gasket Post Placement Type Bolt Bolt Post Placement Type Stud Stud Post Placement Type Nut Nut Post Placement Type Washer Washer Post Placement Type Weldring Weld Ring Post Placement Type Ringjoint Ring Joint Post Placement Type Unknown Unknown Type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-