PortCreateRotationVector Enumeration¶
NXOpen.Routing.Port.CreateRotationVector is an alias for NXOpen.Routing.PortCreateRotationVector
-
class
NXOpen.Routing.
PortCreateRotationVector
¶ Bases:
object
Used by
NXOpen.Routing.FittingPortCollection.CreateFromCsys()
andRouting.FixturePortCollection.CreateFromCsys()
to determine if the rotation vector on the port should be created.Enum Members
Enum Member Enum Member Description No Do not create the rotation vector on the port created from a coordinate system. Yes Create the rotation vector on the port created from a coordinate system. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-