PortConnectionOverriddenValidity Enumeration¶
NXOpen.Routing.PortConnection.OverriddenValidity is an alias for NXOpen.Routing.PortConnectionOverriddenValidity
-
class
NXOpen.Routing.
PortConnectionOverriddenValidity
¶ Bases:
object
Overridden port connection validity
Enum Members
Enum Member Enum Member Description NotSet The port connection validity has not been overridden Valid The port connection validity has been overridden to be valid Invalid The port connection validity has been overridden to be invalid -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-