PointDefinition Enumeration¶
-
class
NXOpen.Routing.
PointDefinition
¶ Bases:
object
Available definitions for the point location for the Point and Length application method Enum Members
Enum Member Enum Member Description Start The point defines the start of the overstock application. Middle The point defines the middle of the overstock application. End The point defines the end of the overstock application. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-