PlatformCreatorBuilderReferenceType Enumeration

NXOpen.Routing.PlatformCreatorBuilder.ReferenceType is an alias for NXOpen.Routing.PlatformCreatorBuilderReferenceType

class NXOpen.Routing.PlatformCreatorBuilderReferenceType

Bases: object

The grate orientation symbol reference

Enum Members

Enum Member Enum Member Description
Horizontal
Vertical
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.