MiteredBendCornerCollection Class¶
-
class
NXOpen.Routing.
MiteredBendCornerCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.MiteredBendCorner
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX9.0.2.
Methods¶
Method | Description |
---|---|
CreateCorner | Create a mitered bend corner object at a Control Point. |
GetBendAssociatedToSegment | Enquire the Mitered Bend Corner that this segment represents. |
Method Detail¶
CreateCorner¶
-
MiteredBendCornerCollection.
CreateCorner
¶ Create a mitered bend corner object at a Control Point.
Signature
CreateCorner(rcp, bendRadius, numberOfMiters)
Parameters: - rcp (
NXOpen.Routing.ControlPoint
) – - bendRadius (float) – Radius of bend corner arc, Must be greater than zero.
- numberOfMiters (int) –
Returns: The new mitered bend corner.
Return type: New in version NX9.0.2.
License requirements: routing_base (“Routing Basic”)
- rcp (
GetBendAssociatedToSegment¶
-
MiteredBendCornerCollection.
GetBendAssociatedToSegment
¶ Enquire the Mitered Bend Corner that this segment represents.
(None can be returned, indicating that this segment does not represent a Bend Corner.)
Signature
GetBendAssociatedToSegment(segment)
Parameters: segment ( NXOpen.Routing.ISegment
) – Segment being queried for the Bend Corner it represents.Returns: Bend Corner that segment represents (None can be returned,indicating that segment does not represent a Bend Corner). :rtype:
NXOpen.Routing.BendCorner
New in version NX9.0.2.
License requirements: routing_base (“Routing Basic”)