InterfaceTerminalRelationshipCollection Class¶
-
class
NXOpen.Routing.
InterfaceTerminalRelationshipCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.InterfaceTerminalRelationshipShadow
objects.See NX Routing help for the Connectivity data model documentation.
To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.2.
Methods¶
Method | Description |
---|---|
CreateElectricalInterfaceTerminalRelationship | Creates and returns a NXOpen.Routing.InterfaceTerminalRelationshipShadow object under electrical data root object. |
CreateMechanicalInterfaceTerminalRelationship | Creates and returns a NXOpen.Routing.InterfaceTerminalRelationshipShadow object under mechanical data root object. |
Method Detail¶
CreateElectricalInterfaceTerminalRelationship¶
-
InterfaceTerminalRelationshipCollection.
CreateElectricalInterfaceTerminalRelationship
¶ Overloaded method CreateElectricalInterfaceTerminalRelationship
CreateElectricalInterfaceTerminalRelationship()
CreateElectricalInterfaceTerminalRelationship(guid)
-------------------------------------
Creates and returns a
NXOpen.Routing.InterfaceTerminalRelationshipShadow
object under electrical data root object.Signature
CreateElectricalInterfaceTerminalRelationship()
Returns: Return type: NXOpen.Routing.InterfaceTerminalRelationshipShadow
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates and returns a
NXOpen.Routing.InterfaceTerminalRelationshipShadow
object under electrical data root object.Signature
CreateElectricalInterfaceTerminalRelationship(guid)
Parameters: guid (str) – Unique Identifier, NX will generate guid, if the value is NULL Returns: Return type: NXOpen.Routing.InterfaceTerminalRelationshipShadow
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
CreateMechanicalInterfaceTerminalRelationship¶
-
InterfaceTerminalRelationshipCollection.
CreateMechanicalInterfaceTerminalRelationship
¶ Overloaded method CreateMechanicalInterfaceTerminalRelationship
CreateMechanicalInterfaceTerminalRelationship()
CreateMechanicalInterfaceTerminalRelationship(guid)
-------------------------------------
Creates and returns a
NXOpen.Routing.InterfaceTerminalRelationshipShadow
object under mechanical data root object.Signature
CreateMechanicalInterfaceTerminalRelationship()
Returns: Return type: NXOpen.Routing.InterfaceTerminalRelationshipShadow
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates and returns a
NXOpen.Routing.InterfaceTerminalRelationshipShadow
object under mechanical data root object.Signature
CreateMechanicalInterfaceTerminalRelationship(guid)
Parameters: guid (str) – Unique Identifier, NX will generate guid, if the value is NULL Returns: Return type: NXOpen.Routing.InterfaceTerminalRelationshipShadow
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------