InterfaceTerminalRelationshipBaseRelationType Enumeration¶
NXOpen.Routing.InterfaceTerminalRelationshipBase.RelationType is an alias for NXOpen.Routing.InterfaceTerminalRelationshipBaseRelationType
-
class
NXOpen.Routing.
InterfaceTerminalRelationshipBaseRelationType
¶ Bases:
object
Type of interface terminal relationships as per STEP 212 Standards. Currently, only decomposition is implemented, other types will be added in future releases as required.
New in version NX4.0.2.
Enum Members
Enum Member Enum Member Description Decomposition -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-