IntegrateRunsBuilderEnum Enumeration

NXOpen.Routing.IntegrateRunsBuilder.Enum is an alias for NXOpen.Routing.IntegrateRunsBuilderEnum

class NXOpen.Routing.IntegrateRunsBuilderEnum

Bases: object

RunAttributes from which Run

Enum Members

Enum Member Enum Member Description
FirstRun
SecondRun
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.