ICharacteristic Class¶
-
class
NXOpen.Routing.
ICharacteristic
¶ Bases:
NXOpen.INXObject
Interface for querying and setting characteristic (UG attribute values) on various routing objects.
These methods should be used instead of the attribute methods on the
NXObject
object in order to support extra functionality such as synonym characteristics available in the Routing application. .. versionadded:: NX4.0.0