Methods¶
Method | Description |
---|---|
CreateFilter | Creates a NXOpen.Routing.Electrical.ElectricalNavigatorFilter object. |
GetDisplayFilter | Get the displayed NXOpen.Routing.Electrical.ElectricalNavigatorFilter object for the given navigator type |
SetDisplayFilter | Set the NXOpen.Routing.Electrical.ElectricalNavigatorFilter object as displayed filter for given navigator type. |
Method Detail¶
CreateFilter¶
Creates a
NXOpen.Routing.Electrical.ElectricalNavigatorFilter
object.Signature
CreateFilter(name, clause)
Parameters: - name (str) – Name of the filter
- clause (str) – Clause of the filter
Returns: Return type: New in version NX5.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetDisplayFilter¶
Get the displayed
NXOpen.Routing.Electrical.ElectricalNavigatorFilter
object for the given navigator typeSignature
GetDisplayFilter(type)
Parameters: type ( NXOpen.Routing.Electrical.ElectricalFormatType
) –Returns: Return type: NXOpen.Routing.Electrical.ElectricalNavigatorFilter
New in version NX5.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetDisplayFilter¶
Set the
NXOpen.Routing.Electrical.ElectricalNavigatorFilter
object as displayed filter for given navigator type.Signature
SetDisplayFilter(type, filter)
Parameters: New in version NX5.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)