ElectricalFormatCollection Class¶
-
class
NXOpen.Routing.Electrical.
ElectricalFormatCollection
¶ Bases:
object
Represents a Routing
NXOpen.Routing.Electrical.ElectricalFormatCollection
object.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX5.0.1.
Methods¶
Method | Description |
---|---|
CreateFormat | Creates a NXOpen.Routing.Electrical.ElectricalFormat object. |
GetDisplayFormat | Get the displayed NXOpen.Routing.Electrical.ElectricalFormat object for the given navigator type. |
SetDisplayFormat | Set the NXOpen.Routing.Electrical.ElectricalFormat object as displayed format for the given navigator type. |
Method Detail¶
CreateFormat¶
-
ElectricalFormatCollection.
CreateFormat
¶ Creates a
NXOpen.Routing.Electrical.ElectricalFormat
object.Signature
CreateFormat(name, type)
Parameters: - name (str) –
- type (
NXOpen.Routing.Electrical.ElectricalFormatType
) –
Returns: Return type: New in version NX5.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetDisplayFormat¶
-
ElectricalFormatCollection.
GetDisplayFormat
¶ Get the displayed
NXOpen.Routing.Electrical.ElectricalFormat
object for the given navigator type.Signature
GetDisplayFormat(type)
Parameters: type ( NXOpen.Routing.Electrical.ElectricalFormatType
) –Returns: Return type: NXOpen.Routing.Electrical.ElectricalFormat
New in version NX5.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetDisplayFormat¶
-
ElectricalFormatCollection.
SetDisplayFormat
¶ Set the
NXOpen.Routing.Electrical.ElectricalFormat
object as displayed format for the given navigator type.Signature
SetDisplayFormat(type, format)
Parameters: New in version NX5.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)