CablewaysLayoutViewCollection Class¶
-
class
NXOpen.Routing.Electrical.
CablewaysLayoutViewCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.Electrical.CablewaysLayoutView
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CreateLayoutView | Creates NXOpen.Routing.Electrical.CablewaysLayoutView object. |
Method Detail¶
CreateLayoutView¶
-
CablewaysLayoutViewCollection.
CreateLayoutView
¶ Creates
NXOpen.Routing.Electrical.CablewaysLayoutView
object.Only one
NXOpen.Routing.Electrical.CablewaysLayoutView
object can exist per segment, so if the object already exists, it returns the same.Signature
CreateLayoutView(segment)
Parameters: segment ( NXOpen.Curve
) – Segment on which layout view should be created or whose view is asked.Returns: Return type: NXOpen.Routing.Electrical.CablewaysLayoutView
New in version NX7.5.0.
License requirements: routing_cabling (“Routing Cabling”)