AssignProxyBuilder Class¶
-
class
NXOpen.Routing.Electrical.
AssignProxyBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Routing.Electrical.AssignProxyBuilder
.This is used to create a proxy port and assign it to a connector.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateAssignProxyBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Point | Returns or sets the position of the proxy port to be created. |
Tag | Returns the Tag for this object. |
Vector | Returns or sets the direction of the proxy port to be created. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Point¶
-
AssignProxyBuilder.
Point
¶ Returns or sets the position of the proxy port to be created.
-------------------------------------
Getter Method
Signature
Point
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Point
Parameters: point ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Vector¶
-
AssignProxyBuilder.
Vector
¶ Returns or sets the direction of the proxy port to be created.
-------------------------------------
Getter Method
Signature
Vector
Returns: Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Vector
Parameters: vector ( NXOpen.Direction
) –New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
Validate¶
-
AssignProxyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.