EditPlacePartBuilder Class¶
-
class
NXOpen.Routing.
EditPlacePartBuilder
¶ Bases:
NXOpen.Builder
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateEditPlacePartBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
SelectedPart | Returns the target body to edit part placement |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FinalizePlacementForScrewSeat | Places a screw measurement holder seat part onto a target object by locating and constraining by the given parameters. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetScrewSeatAngle | Gets the angle expression to be used for screw seat placement along a placed object. |
GetScrewSeatLength | Gets the length expression to be used for screw seat placement along a placed object. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectedPart¶
-
EditPlacePartBuilder.
SelectedPart
¶ Returns the target body to edit part placement
-------------------------------------
Getter Method
Signature
SelectedPart
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX10.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
FinalizePlacementForScrewSeat¶
-
EditPlacePartBuilder.
FinalizePlacementForScrewSeat
¶ Places a screw measurement holder seat part onto a target object by locating and constraining by the given parameters.
Signature
FinalizePlacementForScrewSeat(startPointId, endPointId, alignStartPoint, alignEndPoint, length, angle, alignVector, screwSeatInstance, target)
Parameters: - startPointId (
NXOpen.TaggedObject
) – The starting input point - endPointId (
NXOpen.TaggedObject
) – The end input point - alignStartPoint (
NXOpen.Point3d
) – The starting point to align screw seat fixture port at - alignEndPoint (
NXOpen.Point3d
) – The ending point to align screw seat fixture port at - length (
NXOpen.Expression
) – The length along target to place screw seat - angle (
NXOpen.Expression
) – The angle along target to place screw seat - alignVector (
NXOpen.Vector3d
) – The align vector along which to position screw seat - screwSeatInstance (
NXOpen.TaggedObject
) – The screw seat instance to constrain to - target (
NXOpen.TaggedObject
) – The target object to constrain to
New in version NX10.0.0.
License requirements: routing_base (“Routing Basic”)
- startPointId (
GetScrewSeatAngle¶
-
EditPlacePartBuilder.
GetScrewSeatAngle
¶ Gets the angle expression to be used for screw seat placement along a placed object.
Signature
GetScrewSeatAngle()
Returns: The angle used for screw seat placement on placed routing object. Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: routing_base (“Routing Basic”)
GetScrewSeatLength¶
-
EditPlacePartBuilder.
GetScrewSeatLength
¶ Gets the length expression to be used for screw seat placement along a placed object.
Signature
GetScrewSeatLength()
Returns: The length used for screw seat placement on placed routing object. Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
EditPlacePartBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.