DivisionsBuilder Class¶
-
class
NXOpen.Routing.
DivisionsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Routing.DivisionsBuilder
Builder for creating/editing splits at an end of a duct.
Takes an end face of a rectangular stock and splits it into a pair of divisions based on the specified absolute flow percentage for each division.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateDivisionsBuilder()
Default values.
Property Value LeftChildFlow.Value 50 RightChildFlow.Value 50 SplitDirection SplitVertically New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
LeftChildFlow | Returns the value of percent absolute or relative flow in left (first) child division |
RightChildFlow | Returns the value of percent absolute or relative flow in right (second) child division |
SelectedPort | Returns the NXOpen.Routing.Port to identify the cross-section that is to be split |
SplitDirection | Returns or sets the direction of split, either vertical or horizontal |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateDivisions | Creates two new divisions by splitting the parent division. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDivision | Gets the division object, if any, associated with the division builder |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DivisionsBuilderSplitDirectionType Enumeration | The direction in which the cross-section is to be split |
Property Detail¶
LeftChildFlow¶
-
DivisionsBuilder.
LeftChildFlow
¶ Returns the value of percent absolute or relative flow in left (first) child division
-------------------------------------
Getter Method
Signature
LeftChildFlow
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_hvac (“Routing HVAC”)
RightChildFlow¶
-
DivisionsBuilder.
RightChildFlow
¶ Returns the value of percent absolute or relative flow in right (second) child division
-------------------------------------
Getter Method
Signature
RightChildFlow
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_hvac (“Routing HVAC”)
SelectedPort¶
-
DivisionsBuilder.
SelectedPort
¶ Returns the
NXOpen.Routing.Port
to identify the cross-section that is to be split-------------------------------------
Getter Method
Signature
SelectedPort
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.0.
License requirements: routing_hvac (“Routing HVAC”)
SplitDirection¶
-
DivisionsBuilder.
SplitDirection
¶ Returns or sets the direction of split, either vertical or horizontal
-------------------------------------
Getter Method
Signature
SplitDirection
Returns: Return type: NXOpen.Routing.DivisionsBuilderSplitDirectionType
New in version NX7.5.0.
License requirements: routing_hvac (“Routing HVAC”)
-------------------------------------
Setter Method
Signature
SplitDirection
Parameters: splitDirection ( NXOpen.Routing.DivisionsBuilderSplitDirectionType
) –New in version NX7.5.0.
License requirements: routing_hvac (“Routing HVAC”)
Method Detail¶
CreateDivisions¶
-
DivisionsBuilder.
CreateDivisions
¶ Creates two new divisions by splitting the parent division.
Signature
CreateDivisions()
Returns: Return type: NXOpen.Routing.Division
New in version NX7.5.0.
License requirements: routing_hvac (“Routing HVAC”)
GetDivision¶
-
DivisionsBuilder.
GetDivision
¶ Gets the division object, if any, associated with the division builder
Signature
GetDivision()
Returns: Return type: NXOpen.Routing.Division
New in version NX7.5.0.
License requirements: routing_hvac (“Routing HVAC”)
Validate¶
-
DivisionsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.