DeviceRelationshipRelationType Enumeration¶
NXOpen.Routing.DeviceRelationship.RelationType is an alias for NXOpen.Routing.DeviceRelationshipRelationType
-
class
NXOpen.Routing.
DeviceRelationshipRelationType
¶ Bases:
object
Specifies the nature of the relationship between the related and relating objects.
New in version NX4.0.2.
Enum Members
Enum Member Enum Member Description AssociatedEquipment the related single devices are attached to the relating single device -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-