DesignRuleViolationViewerOverrideOption Enumeration¶
NXOpen.Routing.DesignRuleViolationViewer.OverrideOption is an alias for NXOpen.Routing.DesignRuleViolationViewerOverrideOption
-
class
NXOpen.Routing.
DesignRuleViolationViewerOverrideOption
¶ Bases:
object
Enumerations to show options for override
Enum Members
Enum Member Enum Member Description Yes this shows that current violation is overridden violations No this shows that current violation is not overridden. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-