DesignRuleViolationViewerFilterOption Enumeration¶
NXOpen.Routing.DesignRuleViolationViewer.FilterOption is an alias for NXOpen.Routing.DesignRuleViolationViewerFilterOption
-
class
NXOpen.Routing.
DesignRuleViolationViewerFilterOption
¶ Bases:
object
Enumerations to show options for filter.
Enum Members
Enum Member Enum Member Description AllViolations will show all violations SkipOverrides will not show overridden violations OverridesOnly will show only overridden violations -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-