CustomManagerSelectionType Enumeration¶
NXOpen.Routing.CustomManager.SelectionType is an alias for NXOpen.Routing.CustomManagerSelectionType
-
class
NXOpen.Routing.
CustomManagerSelectionType
¶ Bases:
object
Used by the navigator object selected plugin to indicate whether the objects are selected or deselected.
Enum Members
Enum Member Enum Member Description Deselected The objects were deselected. Selected The objects were selected. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-