CustomManagerNavigatorType Enumeration¶
NXOpen.Routing.CustomManager.NavigatorType is an alias for NXOpen.Routing.CustomManagerNavigatorType
-
class
NXOpen.Routing.
CustomManagerNavigatorType
¶ Bases:
object
Used by the navigator object selected plugin to indicate in which navigator the objects were selected.
Enum Members
Enum Member Enum Member Description Component The objects were selected in the component navigator. Connection The objects were selected in the connection navigator. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-