CustomManagerDuctSizeCalculatorDisplayNoteFlag Enumeration¶
NXOpen.Routing.CustomManager.DuctSizeCalculatorDisplayNoteFlag is an alias for NXOpen.Routing.CustomManagerDuctSizeCalculatorDisplayNoteFlag
-
class
NXOpen.Routing.
CustomManagerDuctSizeCalculatorDisplayNoteFlag
¶ Bases:
object
Used by the Duct Size Calculator’s display note plugin to indicate whether to add or remove the note.
Enum Members
Enum Member Enum Member Description AddNote RemoveNote -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-