CornerTypeBuilderType Enumeration¶
NXOpen.Routing.CornerTypeBuilder.Type is an alias for NXOpen.Routing.CornerTypeBuilderType
-
class
NXOpen.Routing.
CornerTypeBuilderType
¶ Bases:
object
Defines the type of bend available for bend creation.Type of bend available are None,Miter ,Bend , S-bend and S-Elbow.
Enum Members
Enum Member Enum Member Description NotSet Miter Bend SBend SElbow UBend UElbow Cope MiteredBend -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-