CornerCollection Class¶
-
class
NXOpen.Routing.
CornerCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.Corner
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
GetRcpCornerInfo | Gets the corner information given a NXOpen.Routing.ControlPoint . |
Method Detail¶
GetRcpCornerInfo¶
-
CornerCollection.
GetRcpCornerInfo
¶ Gets the corner information given a
NXOpen.Routing.ControlPoint
.Signature
GetRcpCornerInfo(rcp)
Parameters: rcp ( NXOpen.Routing.ControlPoint
) – Object to interrogateReturns: a tuple Return type: A tuple consisting of (corner, cornerType). corner is a NXOpen.Routing.Corner
.NXOpen.Routing.Corner
associated with this RCP cornerType is aNXOpen.Routing.CornerType
. Type of corner.New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)