ControlPointCollectionCheckExisting Enumeration¶
NXOpen.Routing.ControlPointCollection.CheckExisting is an alias for NXOpen.Routing.ControlPointCollectionCheckExisting
-
class
NXOpen.Routing.
ControlPointCollectionCheckExisting
¶ Bases:
object
Option for searching for an existing
NXOpen.Routing.ControlPoint
when attempting to create an newNXOpen.Routing.ControlPoint
.Enum Members
Enum Member Enum Member Description DontSearch Don’t search for an exising object, always create a new object. Search Search for an existing object, don’t create a new object if one exists at the correct location. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-