ConnectedCurvesBuilder Class¶
-
class
NXOpen.Routing.
ConnectedCurvesBuilder
¶ Bases:
NXOpen.Builder
Builder for creating automatically creating segments on end-to-end connected curves.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateConnectedCurvesBuilder()
Default values.
Property Value AllowArcs 1 AllowLines 1 AllowOccs 1 AllowSplines 1 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AllowArcs | Returns or sets the flag that allows traversal of arcs when finding connected curves. |
AllowLines | Returns or sets the flag that allows traversal of lines when finding connected curves. |
AllowOccs | Returns or sets the flag that allows traversal of curve occurrences when finding connected curves. |
AllowSplines | Returns or sets the flag that allows traversal of splines when finding connected curves. |
CurveSelection | Returns the list of selected curves. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ChainSelectedCurves | Finds all curves attached end-to-end with the current list of selected curves. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AllowArcs¶
-
ConnectedCurvesBuilder.
AllowArcs
¶ Returns or sets the flag that allows traversal of arcs when finding connected curves.
If False, the traversal will stop when it hits an arc curve. In addition the curve selection list will not allow arcs to be added to the list.
-------------------------------------
Getter Method
Signature
AllowArcs
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AllowArcs
Parameters: allowArcs (bool) – New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
AllowLines¶
-
ConnectedCurvesBuilder.
AllowLines
¶ Returns or sets the flag that allows traversal of lines when finding connected curves.
If False, the traversal will stop when it hits a line curve. In addition the curve selection list will not allow lines to be added to the list.
-------------------------------------
Getter Method
Signature
AllowLines
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AllowLines
Parameters: allowLines (bool) – New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
AllowOccs¶
-
ConnectedCurvesBuilder.
AllowOccs
¶ Returns or sets the flag that allows traversal of curve occurrences when finding connected curves.
If False, the traversal will stop when it hits a curve occurrence. In addition the curve selection list will not allow curve occurrences to be added to the list.
-------------------------------------
Getter Method
Signature
AllowOccs
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AllowOccs
Parameters: allowOccs (bool) – New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
AllowSplines¶
-
ConnectedCurvesBuilder.
AllowSplines
¶ Returns or sets the flag that allows traversal of splines when finding connected curves.
If False, the traversal will stop when it hits an spline curve. In addition the curve selection list will not allow splines to be added to the list.
-------------------------------------
Getter Method
Signature
AllowSplines
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AllowSplines
Parameters: allowSplines (bool) – New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
CurveSelection¶
-
ConnectedCurvesBuilder.
CurveSelection
¶ Returns the list of selected curves.
-------------------------------------
Getter Method
Signature
CurveSelection
Returns: Return type: NXOpen.SelectCurveList
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
ChainSelectedCurves¶
-
ConnectedCurvesBuilder.
ChainSelectedCurves
¶ Finds all curves attached end-to-end with the current list of selected curves.
The returned list of curves includes the selected curves.
Signature
ChainSelectedCurves()
Returns: Return type: list of NXOpen.Curve
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
ConnectedCurvesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.