ConnectPathBuilder Class¶
-
class
NXOpen.Routing.
ConnectPathBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Routing.ConnectPathBuilder
.Routing.ConnectPathBuilderis used to control the connecting of Routing.ControlPoints within the distance tolerance specified. This eliminates duplicate Routing.ControlPoints such that only one Routing.ControlPoint remains. The Routing.Segments that were defined by the duplicate Routing.ControlPoints are now defined by the remaining Routing.ControlPoint. Routing.ConnectPath is the reverse operation to Routing.DiscontinuityCorner. To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateConnectPathBuilder()
Default values.
Property Value Tolerance 0.01 (millimeters part), 0.001 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Selection | Returns the Routing. |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the 3D distance within which Routing. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Selection¶
-
ConnectPathBuilder.
Selection
¶ Returns the Routing.
ControlPoints that are selected.
-------------------------------------
Getter Method
Signature
Selection
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
Tolerance¶
-
ConnectPathBuilder.
Tolerance
¶ Returns or sets the 3D distance within which Routing.
ControlPoints will be considered duplicates and some will be merged away so that only one Routing.ControlPoint remains.
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tolerance (float) – New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
Validate¶
-
ConnectPathBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.