CompareRunsBuilderCompareTypes Enumeration

NXOpen.Routing.CompareRunsBuilder.CompareTypes is an alias for NXOpen.Routing.CompareRunsBuilderCompareTypes

class NXOpen.Routing.CompareRunsBuilderCompareTypes

Bases: object

The Compare Type selection Enum.

Enum Members

Enum Member Enum Member Description
Xml
Part
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.