BranchPathNumberingBuilderSequence Enumeration¶
NXOpen.Routing.BranchPathNumberingBuilder.Sequence is an alias for NXOpen.Routing.BranchPathNumberingBuilderSequence
-
class
NXOpen.Routing.
BranchPathNumberingBuilderSequence
¶ Bases:
object
Specifies the sequence method
Enum Members
Enum Member Enum Member Description Numbers 1, 2, 3, and so on UpperCase A, B, C, and so on LowerCase a, b, c, and so on -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-