BendReportManagerYbcReport_Struct Struct¶
NXOpen.Routing.BendReportManager.YbcReport is an alias for NXOpen.Routing.BendReportManagerYbcReport_Struct
-
class
NXOpen.Routing.
BendReportManagerYbcReport_Struct
¶ Bases:
object
Used in the YBC bend reports.
The last bend value isn’t actually a bend. The only valid value is the Y value, which is the length after the last bend. All values are relative, meaning they are calculated from the previous bend. So if bend1 has B value of 90 degrees and bend2 has a B value of 90 degrees, then the pipe has rotated 180 degrees about the Y axis. . Constructor: NXOpen.Routing.BendReportManager.YbcReport()
Fields¶
Field | Description |
---|---|
NXOpen.Routing.BendReportManagerYbcReport_Struct.Y | The length along the stock before the bend. |
NXOpen.Routing.BendReportManagerYbcReport_Struct.B | The rotation angle in degrees about the Y axis of the stock. |
NXOpen.Routing.BendReportManagerYbcReport_Struct.C | The rotation angle in degrees about the Z axis of the stock. |
Radius | Radius of the bend. |
Y¶
-
BendReportManagerYbcReport_Struct.
Y
¶ The length along the stock before the bend.
-------------------------------------
Field Value Type:float