BendReportManagerXyzReport_Struct Struct¶
NXOpen.Routing.BendReportManager.XyzReport is an alias for NXOpen.Routing.BendReportManagerXyzReport_Struct
-
class
NXOpen.Routing.
BendReportManagerXyzReport_Struct
¶ Bases:
object
Used in the XYZ bend reports.
The first bend value is at one end point of the stock body and the last bend value is at the other end point of the stock body. The other bend values are the location in work coordinates of the bend :py:class:`Routing.ControlPoint`s associated with each bend or the location of where the bend :py:class:`Routing.ControlPoint`s would be if they existed. . Constructor: NXOpen.Routing.BendReportManager.XyzReport()
Fields¶
Field | Description |
---|---|
Xc | X position of bend Routing.ControlPoint in work coordinates. |
Yc | Y position of bend Routing.ControlPoint in work coordinates. |
Zc | Z position of bend Routing.ControlPoint in work coordinates. |
Radius | Radius of the bend. |
Xc¶
-
BendReportManagerXyzReport_Struct.
Xc
¶ X position of bend
Routing.ControlPoint
in work coordinates.-------------------------------------
Field Value Type:float
Yc¶
-
BendReportManagerXyzReport_Struct.
Yc
¶ Y position of bend
Routing.ControlPoint
in work coordinates.-------------------------------------
Field Value Type:float